STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB-C Key detection

Hello, I am working on a Bootloader that reads USB-Key using USB_Host middleware to retrieve files before performing some operations but I have some issues detecting some USB keys.USB 2.0 Keys are all detectedUSB 3.2 Keys are not well detectedI have ...

SKham.2 by Associate II
  • 3682 Views
  • 11 replies
  • 2 kudos

Resolved! STM32G4 FW 1.5.2 FDCan Error/Bug?

Hi guys I've upgraded from 1.5.1 to 1.5.2 and I'm receiving HardFaults when using FDCAN \STM32Cube\Repository\STM32Cube_FW_G4_V1.5.1\Drivers\STM32G4xx_HAL_Driver\Src\stm32g4xx_hal_fdcan.c FW 1.5.1 Line: 3493     /* Write Tx payload to the message RAM...

Framet by Associate III
  • 4401 Views
  • 6 replies
  • 2 kudos

stm32 FDCAN bootloader

Hello ST Community,We are using the STM32G0B1RET6 and have created a custom bootloader using FDCAN. Our setup includes two separate STM32CubeIDE projects:Bootloader ProjectProgrammed via ST-LINK V2Receives application firmware over FDCANWrites it to ...

AKG123 by Associate III
  • 1313 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F334R8 ADC problem

Hello everyone! I am trying to use the ADC of my NUCLEO-F334R8 board. I want to read the PC1 pin (ADC12, channel 7). I try to initialize the ADC with the following code: void BSP_ADC_Init() { // Enable GPIOC clock RCC->AHBENR |= RCC_AHBENR_G...

Santos by Associate II
  • 3753 Views
  • 9 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.