STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7, Hard fault in USBH_MSC_GetLUNInfo()

Hi,I have a STM32F7 and I use USB MSC without RTOS.When debugging with JTAG after connecting the USB memory, a hard fault occurs as follows.*Check Appli_state = APPLICATION_START in USBH_UserProcess() before f_mount()HAL version(MCU package): 1.17.2 ...

Hosung_0-1745898495580.png
Hosung by Associate II
  • 1418 Views
  • 3 replies
  • 0 kudos

STM32G0B1 USB Custom HID

Hi, I am working with STM32G0B1CETx for an application as a replacement of STM32F105VCTx. I want to use to USB as Custom Human Interface Device Class. I am using CubeMx with MDK-ARM. I have configured USB_DRD_FS as Device_only_FS and Middleware secti...

SPK_FW by Associate II
  • 3010 Views
  • 8 replies
  • 1 kudos

Resolved! STM32CubeMX CMake project build error

Hello,I am creating a CMake project using STM32CubeMX 6.13.0 for the STM32U575QGI6Q, but am having trouble with the following error: [1/10] Building ASM object CMakeFiles/rtm.dir/Middlewares/...x/ports/cortex_m33/gnu/src/tx_thread_context_restore.S.o...

JFisher by Associate II
  • 2807 Views
  • 7 replies
  • 4 kudos

AN4457 UART Emulation - use via CubeMx?

Split from old (2020), abandoned thread: https://community.st.com/t5/stm32cubemx-mcus/uart-emulation-an4457-is-it-possible-to-use-it-via-cubemx/td-p/310812 for better visibility - and to enable marking a solution...Hi,I have the same problem, trying ...

JR72 by Associate
  • 1021 Views
  • 2 replies
  • 2 kudos

Resolved! STM32F4 USBX CDC-ACM Bulk IN endpoint Stall

I am looking for help solving a CDC-ACM problem with Azure Rtos ThreadX, and the USBX Middleware for STM32F4.My device is an STM32F427VGTx.I currently have a project that uses the USBX host library. I am connecting up to 4x CDC-ACM devices through an...

akorsich by Associate II
  • 1577 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.