STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Issue with HAL_Delay() and ThreadX

Hello everyone,I am encountering an issue with the HAL_Delay() function and ThreadX in my project. Before initializing ThreadX, HAL_Delay() works as expected. Specifically, the callback function:void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *h...

JonConesa by Associate III
  • 1906 Views
  • 3 replies
  • 1 kudos

STM32H743 USB device transmits zeros to the Host

Everything else is working fine.Setup packet with SET_ADDRESS received and processed.Next GET_DESCRIPTOR for DEVICE which is sent back ok I've verified the data written to the Tx FIFO is correct.Correct number of bytes it transmitted but the bytes ar...

usb-view-cap1.png
lw23 by Associate
  • 1463 Views
  • 3 replies
  • 0 kudos

Resolved! FDCAN: Retransmissions Configuration

Good afternoonI am working on the STM32H755 and am dealing with the retransmissions from my CAN FD periphery. According to the ISO-11898-1:2024 standard, the number of retransmissions should be configurable:"- from 0 (no retransmission),- to at least...

MFrie.7 by Associate III
  • 3919 Views
  • 9 replies
  • 2 kudos

Resolved! HAL_ADC_ConvCpltCallback only gets called once

I'm setting up the ADC in "manual continuous" mode where hadc1.Init.ContinuousConvMode = DISABLE and then I call HAL_ADC_Start_IT() inside of HAL_ADC_ConvCpltCallback().  I get the first call to HAL_ADC_ConvCpltCallback and calling HAL_ADC_Start_IT()...

HAL I2C abort DMA on I2C error

On an STM32G4, if an I2C error occurs (e.g. a bus error) during a DMA driven I2C transaction, is the intention that the HAL I2C driver abort the DMA transfer?Starting at line 6599 in stm32g4xx_hal_i2c.c (v1.2.5), I see code in the I2C_ITError functio...

mjones37 by Associate
  • 1815 Views
  • 3 replies
  • 0 kudos

Help with simple gamepad USB HID

Hello, for my first project with a microcontroller I'm doing a 16 button gamepad USB HID with the aid of ChatGPT. I have no idea of what I'm doing really. I'm Using a STM32f103C8T6 and  STLink V2. I made a polling version that constantly read pins an...

Masfeo by Associate II
  • 2463 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.