2025-05-08 7:15 AM
Hello everyone,
I am encountering an issue with the HAL_Delay() function and ThreadX in my project. Before initializing ThreadX, HAL_Delay() works as expected. Specifically, the callback function:
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
/* USER CODE BEGIN Callback 0 */
/* USER CODE END Callback 0 */
if (htim->Instance == TIM6)
{
HAL_IncTick();
}
/* USER CODE BEGIN Callback 1 */
WR_TIMER_process();
/* USER CODE END Callback 1 */
}is triggered correctly, and the uwTick variable increments as intended.
I am using Timer6 for the system ticks on a custom PCB with an STM32H743BIT MCU. However, after calling the MX_ThreadX_Init() function, the uwTick variable stops updating, and the HAL_TIM_PeriodElapsedCallback is no longer triggered.
Here is my setup:
MCU: STM32H743BIT
Compiler: arm-none-eabi-gcc (Arm GNU Toolchain 14.2.Rel1 (Build arm-14.52)) 14.2.1 20241119
CubeMX Version: 6.14.0
Debugger: J-Link 8.32
Ozone Version: 3.38g
It seems like the initialization of ThreadX might be interfering with the callback mechanism. Has anyone experienced a similar issue, or does anyone know what could cause the callback to stop triggering after initializing ThreadX?
Thank you for your help!
Solved! Go to Solution.
2025-05-20 2:39 AM
Hi,
The issue occurs when calling HAL_Delay() within the function:
UINT App_ThreadX_Init(VOID *memory_ptr).
I removed the delays that were placed inside this function and moved them to the thread, where they worked correctly.
I understand that certain HAL functions cannot be called until the ThreadX initialization is fully completed.
Best regards,
Jon.
2025-05-08 7:23 AM
2025-05-14 6:50 AM
Any update concerning this issue?
2025-05-20 2:39 AM
Hi,
The issue occurs when calling HAL_Delay() within the function:
UINT App_ThreadX_Init(VOID *memory_ptr).
I removed the delays that were placed inside this function and moved them to the thread, where they worked correctly.
I understand that certain HAL functions cannot be called until the ThreadX initialization is fully completed.
Best regards,
Jon.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.