STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PuTTy not receiving data from UART

Hello,  I am using the STMH753ZI chip on the nucleo 144 board. I cannot figure out why my UART code will not show what I am typing in my putty terminal. Attached is my main.c. Thanks. /* USER CODE BEGIN Header */ /** *******************************...

pb33 by Associate II
  • 2130 Views
  • 10 replies
  • 5 kudos

HAL_ADC_ConvCpltCallback optimized away

Post edited to follow the community rules: Please review how to share a code in this post.Using the stm32g030k8 and the Version: 1.18.1 STM32CubeIDE I just recently applied an optimization in order to get more space for my application firmware. And t...

carlesls2 by Associate III
  • 3909 Views
  • 18 replies
  • 10 kudos

Resolved! ADC external channels doubt

I use the STM32CubeIDE Version: 1.18.1 and the stm32g030k8.I have a hardware that uses a firmware. This firmware correctly returns the values of the ADC. The ADC is linked to a DMA. Channel 4 == 2545 (this is a voltage divisor) 12.5 voltsChannel 10 =...

carlesls2_1-1750147679960.png carlesls2_2-1750148586492.png
carlesls2 by Associate III
  • 1134 Views
  • 3 replies
  • 0 kudos

Resolved! FileX + CMake + CM33 = error

I'm trying to build a STM32U5 (THREADX_ARCH = cortex_m33) project that use FileX (https://github.com/STMicroelectronics/stm32-mw-filex) with CMake.I encounter an error that say "FileX/ports/cortex_m33/gnu" is not an existing directory.Why Cortex m33 ...

nicolas by Senior II
  • 1760 Views
  • 7 replies
  • 0 kudos

Resolved! F769 EVAL QSPI_Executeinplace example code

when running the QSPI_Executeinplace example code on the stm32f769i_eval board,the program enters HardFault_handler() after executing GpioToggle().i just remove the QSPI_DummyCyclesCfg(),in GpioToggle() the GPIO Not Taking effect,so How can I solve t...

NetX Internal Mutex Contention

Hi all, I'm using ThreadX with NetX Duo and running a Modbus TCP server on an STM32 platform. The system works fine under normal conditions, but I encounter a hang when the following sequence occurs: A Modbus TCP client is actively communicating with...

Resolved! NUCLEO F756ZG Netx WebServer NO-FX

Hi,I am testing an application between multiple MCUs, I have an H573, an F756 and an F439.I am testing multiple things at a time, so the code generation is helping me.In the H573 I have the flag for using the webserver without FileX, and it will defi...

coso2 by Associate II
  • 1986 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.