2025-06-16 6:28 AM - last edited on 2025-06-16 8:02 AM by Amel NASRI
when running the QSPI_Executeinplace example code on the stm32f769i_eval board,the program enters HardFault_handler() after executing GpioToggle().i just remove the QSPI_DummyCyclesCfg(),in GpioToggle() the GPIO Not Taking effect,so How can I solve this problem? thanks
Solved! Go to Solution.
2025-06-16 7:58 AM
Hello @andrewpei ,
Use a debugger to identify the exact instruction causing the HardFault.
Have you made any updates to the example? If yes, please share the exact modifications you made and the debugger output when the HardFault occurs?
Ensure that the QSPI and GPIO peripherals do not have conflicting configurations or resource usage.
Ensure that the dummy cycles are correctly configured as per the QSPI memory datasheet.
Remember to use the latest release of CubeF7 firmware package.
2025-06-16 7:58 AM
Hello @andrewpei ,
Use a debugger to identify the exact instruction causing the HardFault.
Have you made any updates to the example? If yes, please share the exact modifications you made and the debugger output when the HardFault occurs?
Ensure that the QSPI and GPIO peripherals do not have conflicting configurations or resource usage.
Ensure that the dummy cycles are correctly configured as per the QSPI memory datasheet.
Remember to use the latest release of CubeF7 firmware package.
2025-06-16 8:11 AM
Hello @andrewpei
Please refer to this article to debug hardfault.
2025-06-16 8:55 PM
Hello,@Imen.D ,
Indeed, by debug the code, I found that the data written to NOR Flash differs from the original data,because the dummy cycle configuration for my NOR Flash under the QUAD_OUT_FAST_READ_CMD instruction differs from the example code's implementation.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.