STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem Interfacing SD Card with STM32H753ZIT6

Hi, I'm facing issues while trying to interface a 32GB SD card with the STM32H753ZIT6 development board using SDMMC1 and FatFS. Below are the key problems observed:SD Initialization Fails:HAL_SD_Init() consistently returns HAL_ERROR (Status: 1).Card ...

Ematic by Associate II
  • 2045 Views
  • 3 replies
  • 0 kudos

USB VCP Get_SerialNum

Hello Everybody, I use STM32CubeIDE1.15.0 Build: 20695_20240315_1429 and a custom board with a STM32303RE inside.I use the IOC interface to set the virtual port com. Everything work fine, just a detail: when i connect, then disconnect and reconnect t...

legalguillaume_0-1711471641088.png legalguillaume_0-1711473139330.png

Resolved! STM32H743AII6 PackageType

Hi, we are currently using different types of the STM32H743 and I want to verify the package to make sure the software is running on the expected device. For this I am using LL_GetPackageType() and check the returned value against one of the LL_UTILS...

Issue with interupts STM32F410RB

Hello,i have configured timer1 to trigger via CC1  an  adc + dma.For the DMA i have  placed the TC irq routine and placed a gpio toggle to follow with a logic analyzer like shown below void DMA2_Stream0_IRQHandler(void){ if (DMA_GetITStatus(DMA2_St...

Bogdan by Senior
  • 1005 Views
  • 4 replies
  • 2 kudos

STM32U575ZI LPTIM1 STOP mode Wake

Hi All,I'm struggling to get LPTIM1 to wake from STOP mode on the STM32U5 series parts. I have a STM32U575ZI Nucleo board. When I use SLEEP mode, the LPTIM1_IRQHandler in stem32u5xx_it.c is hit. When I use STOP mode, it is not. I made an example with...

Jeff Gros by Associate III
  • 1709 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.