2025-06-23 5:51 AM - last edited on 2025-08-26 6:41 AM by Andrew Neil
Hi,
I'm facing issues while trying to interface a 32GB SD card with the STM32H753ZIT6 development board using SDMMC1 and FatFS. Below are the key problems observed:
SD Initialization Fails:
HAL_SD_Init() consistently returns HAL_ERROR (Status: 1).
Card Not Ready:
The card state remains 0, indicating that it is not ready or not properly initialized.
Incorrect Card Capacity Reported:
Despite using a 32GB SD card, the detected capacity is only about 1.8GB (1806848 KB).
This suggests the card isn't being properly initialized or detected, and capacity detection is failing. Looking for help identifying the root cause—whether it's clock config, pin setup, timing issues, or something else.
I have attached the code and output file.
Pin connection between SD card to STM32:
-------------------------------------------------------------
DAT0 -> PC8
DAT1 -> PC9
DAT2 -> PC10
DAT2 -> PC11
CLK -> PC12
CMD -> PD2
VCC -> 3.3V
GND -> GND
2025-07-09 2:50 AM
Hello @Ematic;
Did you get the same issue when working in 1 bit bus wide mode?
Could you try to use the latest STM32CubeMX version to generate your code.
I recommend you to look at How to create a file system on a SD card using STM32CubeIDE - STMicroelectronics Community
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-09 4:02 AM
Hi,
probably your hardware is ....
read in forum:
https://community.st.com/t5/stm32cubemx-mcus/running-sdio-4bit-wide-mode/td-p/804098
...
2025-08-26 6:45 AM - edited 2025-08-26 6:48 AM
@Ematic wrote:the STM32H753ZIT6 development board
Which board, exactly? NUCLEO-H753ZI ?
Have you checked that there's nothing else on the board using the pins you've chosen?
@Ematic wrote:
SD Initialization Fails:
HAL_SD_Init() consistently returns HAL_ERROR (Status: 1).
So have you stepped into that function to find where and why it fails?
@Ematic wrote:3. Incorrect Card Capacity Reported:
If the initialisation has failed, then that's not surprising
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.