STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L USB clock from HSI

Posted on September 13, 2013 at 00:42I'm a little bit confused with clocking scheme of the USB peripheral in STM32L151.On the datasheet, we see this affirmation, below the general clocking scheme of the microcontroller:''For the USB function to be a...

DFU class request in hid class device

Posted on April 01, 2015 at 19:41Hello, I'm implementing my own boot loader code for stm32f4. In this boot loader I want to implement a hid class updater (for device firmware) which accept DFU class specific requests. On the PC side I want to modify...

HAL_FLASH_Program always return error code 0x06

Posted on March 30, 2015 at 15:44I use STM32F417IGMinimal example of code:uint32_t startAddress = 0x80E0000;static uint32_t mSize =0x13;//char test_string[13]={''Hello World.''};HAL_FLASH_Unlock();for(uint32_t i=0;i<mSize;i++){ status = HAL_FLASH_Pr...

chief by Associate II
  • 1664 Views
  • 2 replies
  • 0 kudos

stm32 boot pin configuration

Posted on March 30, 2015 at 16:20Hi, we're using STM32F407VG on our project. When we reset the circuit for BOOT, microcontroller is setting B13 pin (which is not using as boot pins) . How can we stop this situation? Can we make any difference for th...

berat by Associate
  • 1316 Views
  • 1 replies
  • 0 kudos

STM32F42x ROM DFU Descriptor

Posted on March 30, 2015 at 11:32It appears that DFU in the STM32F42x ROM Bootloader has an issue: The device returns a descriptor response string as a malformed packet (according to wireshark) for the @Internal Flash interface. The bLength field in...

Multiple funcs mapped to one Pin

Posted on March 29, 2015 at 00:45Hi,     I am a student studying EE, and do not have any experience in circuit design besides the theory being taught in college and a six month hardware design Co-Op. Currently, I am developing a board to be used for...

ziegler by Associate
  • 1622 Views
  • 3 replies
  • 0 kudos

SPL to CubeF4 conversion issues

Posted on March 27, 2015 at 12:22I need to integrate an old code written using the Standard Peripheral Library to a new (big)project that's using CubeF4.As easy as it sounds I can't find any commonality between the libs..1. Is there any documentatio...

ariel2 by Associate II
  • 2104 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.