2013-09-12 3:42 PM
I'm a little bit confused with clocking scheme of the USB peripheral in STM32L151.
On the datasheet, we see this affirmation, below the general clocking scheme of the microcontroller:''For the USB function to be available, both HSE and PLL must be enabled, with the CPU running at either 24 MHz or 32 MHz.''But, on the user manual, there isn't the same advice, all that i found was the description of PLL on 5.2.4, which tell us that both HSI or HSE can supply the PLL, and that this is whom clock the usb.My question is: Is it really necessary to have the HSE running to use USB peripheral, or HSI + PLL is enough?Thanks in advance! #usb-stm32l2013-09-12 3:58 PM
The HSI does not have the stability/accuracy required to meet the USB spec.
2015-04-02 1:27 AM
Well, in the STM32L151xE STM32L152xE datasheet, paragraph 2.2, it clearly says ''USB crystal-less''. And the errata does not seem to mention that it is a mistake. So these documents should certainly be updated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.