2015-03-25 4:08 AM
I am experimenting STM32 by using a STM32F429I discovery board, with a MEMS on board.
At the moment, any attempt to read the MEMS via SPI by using the Cube libraries has failed. On the other hand, another example project (not Cube based) is working, so the MEMS itself is surely not defective. The initialisation code should be OK because it was generated with CubeMX. Please find here the code I am using, can anyone point me to the error? Also note that I am executing the code with a debugger, so I can actually read the results of the Apologies if my question is stupid, I've started with STM32 only since a few days...command[0] = 0x20; // program control register 1
command[1] = 0x0f; // turn on device if (HAL_SPI_Transmit(&hspi5,command,2,100) != HAL_OK) (... warns the user of a problem and stop) command[0] = 0x8f; // read whoami if (HAL_SPI_Transmit(&hspi5,command,1,100) == HAL_OK) { // result should be 0b11010100 HAL_SPI_Receive(&hspi5,memsBuffer,1,100); whoami = memsBuffer[0]; } #mems #mems #spi #spi #stm32f429i-discovery #stm32cubef42015-03-30 6:16 AM
>The initialisation code should be OK because it was generated with CubeMX.
I assume that you call HAL_SPI_Init(&hspi5) before using SPI (because this is not generated by CubeMX) and that you have selected the correct SPI mode for your sensor:MODE 0:hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;MODE 1:hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;MODE 2:hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;MODE 3:hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;The rest of the code is straightforward.Please note that under /STM32Cube_FW_F4_V1.3.0/Drivers/BSP/STM32F429I-Discovery/ you find MEMS code for your board. There is also a demo available under /STM32Cube_FW_F4_V1.3.0/Drivers/BSP/STM32F429I-Discovery/Hope this helpsPS: I noticed your italian name, I'm too despite my nick.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.