2015-03-15 6:32 PM
Hello everybody,
I'm new with USB devices and I want to develope a Virtual Com Port with STM32L151. I get a example named VirtualComport_loopback for IAR in the packet STM32_USB-FS-Device_Lib_V4.0.0.I have some questions about this example... 1) Archive usb_endp.cWhat is the aim of the function EP3_OUT_CallBack()?I tested the function , and saw what every char I received from the USB Host this function is called, where the char is saved in RAM memory, however always in the first position of the array Receive_Buffer[64]. Is it correct?2) Archive hw_config.cI didn't understand very well the function CDC_Receive_DATA()... inside of this function, there is a function SetEPRxValid(ENDP3), what's the objetive of this line?3) Others EPx_IN/OUT_CallBack functionsAbout the others EPx_IN/OUT_CallBack functions, what is the purpose of them?In the example VirtualComport_loopback, the FW use just the EP3_OUT_CallBack and EP1_IN_CallBack.Thank you very much. #cdc #stm32 #virtual-com-port #usb #vcp2015-03-30 2:40 AM
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/CD00158241.pdf
(STM32 USB-FS-Device development kit).-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.