2017-01-15 7:37 PM
Edit:
Seems as if this wasn't a permanent fix. It still happens ... but why?
I then always have to step through the HAL_Init & sysclockcfg functions until the timer is started. Only then can I resume the program in free running mode.
--------------------
Hi,
I'm using FreeRTOS with TIM14 as clock source on an STM32F2 and I noticed that if I just click restart during a debugging session, it would fail.
After investigating a bit, it seems that the reason is that the tick interrupt register of TIM14 wasn't cleared and therefore the mcu hangs during interrupt enabling in HAL_Init().
To fix this, I swapped SystemClock_Config() and HAL_Init() at the beginning of the main function. Now it works.
Is there any downside to this practice? If not, I suggest using this procedure per default.
Any opinions?
int main(void) {
/* USER CODE BEGIN 1 */
NVIC->ICPR[1] = 0xffffffff; // clear all pending bits
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Configure the system clock */
SystemClock_Config();
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Initialize all configured peripherals */
...
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Note: Line #4 was me trying to clear those bits. Didn't work. But doesn't harm the code either.
#debug #timbase #hang #restart #freertos2017-02-02 5:12 AM
Hi,
I had the same kind of trouble. I modified the vector table offset like this
int main(void)
{/* USER CODE BEGIN 1 */
/* Set the Vector Table base location at 0x08000000 */ //SCB->VTOR = FLASH_BASE | 0x00000; /* Vector Table Relocation in Internal FLASH */ /* USER CODE END 1 *//* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init(); /* Configure the system clock */ SystemClock_Config();....
Otherwise make sure that in file system_stm32f2xx.c VECT_TAB_SRAM is commented
************************* Miscellaneous Configuration ************************/
/*!< Uncomment the following line if you need to use external SRAM mounted on STM322xG_EVAL board as data memory *//* #define DATA_IN_ExtSRAM *//*!< Uncomment the following line if you need to relocate your vector Table in
Internal SRAM. *///#define VECT_TAB_SRAM#define VECT_TAB_OFFSET 0x0000 /*!< Vector Table base offset field. This value must be a multiple of 0x200. *//******************************************************************************/2017-02-06 12:29 PM
Hi
Castrignano.Adalgiso
,thanks for your reply. It seems to work so far. I'll further test it.
Much appreciated!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.