STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bootloader sharing peripheral initialization?

Posted on February 28, 2018 at 00:23The example code for bootloaders and applications both call HAL_Init and SystemClock_Config. I'm guessing that clock initialization is done in both apps because the RCC gets reset in SystemInit.I have tried reusin...

SWD disabling after upload code to STM32F407VET6

Posted on February 25, 2018 at 00:21Hi.I wrote LED blinking code for STM32F407VET6.When I'm using Std_Periph_driver everything is fine. But when I write just CMSIS only led blinking code, after upload hex code to STM32F407VET6 code working, st-link ...

[F767ZI] Sampling and storing Measurement Data

Posted on February 16, 2018 at 01:03Hello!I want to start a project with the NUCLEO-F767ZI soon. In this project I want to measure some quantities with up to 100 kSamples/s and store the data.Would it be physically possible to have the data either s...

Armin L. by Associate II
  • 10084 Views
  • 29 replies
  • 0 kudos

STM32F769I-DISCO: No audio output from wm8994

Posted on October 14, 2017 at 03:33With STM32CubeF7 V1.8.0, there is no audio output from the wm8994 audio chip via the 3.5 mm blue audio output jack on the STM32F769I-Discovery board when parameter OUTPUT_DEVICE_HEADPHONE (or alias OUTPUT_DEVICE_HEA...

JB2500 by Associate III
  • 3669 Views
  • 4 replies
  • 0 kudos

USB OTG MSC B-L475 Board

Posted on February 24, 2018 at 11:09Hi,i have a B-L475 Board and i want to use USB OTG (Host) with a usb stick MSC.Under USB Host in CubeMX i have Drive_VBUS_Fs which Pin have i to choose?#usb-msc-device #stm32-l4

F407 and lis3dsh

Posted on February 23, 2018 at 15:01 I'm try use only registers for lis3dsh. https://community.st.com/external-link.jspa?url=https%3A%2F%2Fgithub.com%2Fmas-kon%2FF407-LIS3DSH - my code. This code sometimes is worked, but sometimes it stopped. C...

COM Port not detected on Windows 7

Posted on February 23, 2018 at 08:09Hello,I am using a STM32F072-EVAL with Atollic TruStudio IDE on Win7 x64 machine.I have started facing virtual com port cannot start (code 10) error since last 3-4 days. Have anyone faced this issue off late and m...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.