2018-02-22 4:42 AM
Hello there,
I am working on MSD Bootloader which I successfully Implemented in STM32F207VETx. However while working I found that t
he default build expect 8.3 format file names, and not Long File Names (LFN).
I tried using LFN by making following changes in ffconf.h
&sharpdefine _CODE_PAGE 437
&sharpdefine _USE_LFN 1 /* 0 to 3 */ / When enable the LFN feature, Unicode handling functions (option/unicode.c) must
/ be added to the project.&sharpdefine _MAX_LFN 40 /* Maximum LFN length to handle (12 to 255) */&sharpdefine _LFN_UNICODE 0 /* 0:ANSI/OEM or 1:Unicode */
&sharpdefine _STRF_ENCODE 0
and getting the following error undefined reference to `ff_convert'
which I think is a function in unicode.c
So My question is where can I Find Unicode handling functions as i want to give a long name for my file
#tilen-majerle #clive-oneSolved! Go to Solution.
2018-02-22 5:23 AM
You might want to migrant to a more current version of FatFS, sounds like you are at 0.09 or something.
You would need to add the CCSBCS.C file to your project to get ff_convert(), ff_wtoupper(), etc
There should be an equivalent in the F2 SPL trees too
\STM32F4xx_DSP_StdPeriph_Lib_V1.8.0\Utilities\Third_Party\fat_fs\src\option\ccsbcs.c
2018-02-22 4:56 AM
Note that FatFs is a 3rd-party product - entirely unrelated to ST.
FatFs documentation is here:
http://elm-chan.org/fsw/ff/00index_e.html
FatFs User Forum:
http://elm-chan.org/fsw/ff/bd/
2018-02-22 5:23 AM
You might want to migrant to a more current version of FatFS, sounds like you are at 0.09 or something.
You would need to add the CCSBCS.C file to your project to get ff_convert(), ff_wtoupper(), etc
There should be an equivalent in the F2 SPL trees too
\STM32F4xx_DSP_StdPeriph_Lib_V1.8.0\Utilities\Third_Party\fat_fs\src\option\ccsbcs.c
2018-02-23 2:10 AM
Thanks Andrew and Clive1 for your support.
Your Answers were really helpful and I successfully changed the default
8.3 format file names to Long File Name(LFN).
I migrated the code from
CCSBCS.C file to my project to get ff_convert(), ff_wtoupper(), and changed the format to my desired length.
However,
I have another question for you, Is it possible that I can download a file in .DFU format using MSD Bootloader as by default it supports .BIN file. If YES then how?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.