2018-02-26 5:39 AM
Hello,
I am using STM32F103 and I would like to use:
STM32F103 USART bootloader + USB as Virtual COM port + PC application for uploading hex file.
My question is: Would it be possible to use embedded USART bootloader (together with STM32-FLASHER) in the following way:
-configure USB as virtual COM port,
-connect with PC, use STM32-FLASHER,
-when program detects USB connection, it jumps from user application into embedded bootloader,
-STM32-FLASHER is used for uploading the code via USB as VPC
As far as I know, before jumping into bootloader we have to disable interrupts and peripherals. But what if I leave USB configured? Would it make any sense to do so? This would save me some work with developing custom bootloader.
#flasher #stm32f103 #usb #bootloader #usb-vcp2018-02-27 1:18 AM
We need to activate the bootloader somehow. This doc shows all the option for many MCUs:
In case of STMF103 probably we do not have option to use the USB as the bootloader 'wire'. For this case I used to develop specill application to be able to load the code through USB.
For newer MCU there is such option. Please see the document I provided the link to.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.