STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeMx LSE drive capability issue

Posted on June 28, 2018 at 17:07I found an issue with the latest (and updated) STM32CubeMx when generating code both for SW4STM32 and for  MDK-ARM relate to STM32F746 board.Changing 'LSE Drive Capability' from ''LSE oscillator low drive capability' ...

STM32L4 - ADC Module using the LL

Posted on June 27, 2018 at 10:18 Hi guys, I'm tryingto use the ADC module of STM32L4 using the Low Level Library. We created a simple project (I have a nucleo board). I used the STM32Cube Mx to generate the Setup Code (the project file is a...

Resolved! Custom STM32F469 board with Standard Peripheral Library 1.8.0: Clock wrong after power up, correct after several resets

Posted on June 27, 2018 at 23:15Hello,I am developing a custom board that mounts a STM32F469 MCU. The board is very simple, and the circuit embeds only the main 8Mhz crystal and the RTC 32.768 one. No embedded peripherals except for a couple of stat...

0690X0000060PHIQA2.jpg 0690X0000060PHmQAM.jpg 0690X0000060PHiQAM.jpg 0690X0000060PHeQAM.jpg
Digimorf by Associate III
  • 1981 Views
  • 3 replies
  • 0 kudos

STM32H7 LwIp Ethernet

Posted on July 03, 2018 at 17:08Hi everyone,I am new to programming Ethernet applications and wanted to start with just sending Ethernet frames with my stm32H7 Nucleo Board. The only Middleware I use is LwIP. My problem is, that the programm itself ...

0690X00000604j4QAA.jpg

IEEE 802.1Q Queuing Frames

Posted on July 03, 2018 at 19:46I'm trying to implement the frames queuing mechanism defined in IEEE 802.1Q standard (section 8.6) on my STM32F7 Nucleo board. It's a well-known layer 2 mechanism that takes place at the outbound Ethernet port and all...

Port AN3966 (HttpServer examples) DevKit407

Posted on July 03, 2018 at 11:02Dear All, I'm trying to work HttpServer with DevKit407 (STM32F407G-DISC1 + STM32F4DIS-BB). I found the AN3966 with examples over STM32F407VG, but it only works over STM3240G-EVAL.Does someone ported AN3966 examples to...

CDC_DATA_FS_MAX_PACKET_SIZE

Posted on July 02, 2018 at 15:32Hi,please help me to understand why when I increase the value of CDC_DATA_FS_MAX_PACKET_SIZE in usbd_cdc.h more than 128 usb communication and the PC both hang??please instruct me what to do to increase the usb receiv...

Problems writing bootloader on STM32107VC

Posted on July 01, 2018 at 11:11I'm working on STM32F107VC and I'm trying to create a simple bootloader.All the boot-loader have to do is check two places in the flash where the application can be and jump to one of the applications.(currently I man...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.