STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 SPI data is sent the reverse way?

Posted on July 09, 2018 at 21:26 I've been experimenting with writing to an external https://www.microchip.com/wwwproducts/en/93LC46B using SPI and I've had mixed success. The data does get shifted out but in an opposite manner. The EEPROM req...

0690X0000060LhcQAE.png

HAL_HCD_IRQHandler only happens once

Posted on June 24, 2018 at 06:41Hi everyone.We have run a project on discovery f746 board consist of FREE RTOS ,  emwin and fat fs sd card library,that it works fine.Now we want to add USB OTG Host in FS mode to our project.We tried to append config...

['F042 USB] USB buffer not writable bytewise

Posted on July 08, 2018 at 16:35RM0091 Rev.9, 30.6.2 Buffer descriptor table, states:The packet memory should be accessed onlyt by byte (8-bit) or half-word (16-bit) accesses.Halfword access is OK. Bytewise read is OK. But writing a byte results in ...

INCLUDE_xTaskAbortDelay

Posted on July 06, 2018 at 16:02This flag should be forced disabled in CubeMX because there is a known bug in FreeRTOS prior to v.10 leading to an out-of-bounds write and (kernel) memory corruption. Must not be used prior to Freertos 10.0.0.#tcb_t #...

STM32L496VG USB CDC(VCP) Receive function

Posted on July 04, 2018 at 05:13 Hello guys. I configure the CDC on CubeMX. But the function CDC_Receive_FS receive1 byte each. That is, if I transmit 12345678 then I receive only 8. I have to modify the function like this: uint8_t UserData...

den2life by Associate II
  • 2389 Views
  • 4 replies
  • 0 kudos

HAL UART Error but no Error Code

Posted on August 07, 2017 at 17:32 Hello, I am getting UART errors (by the means of the HAL_UART_ErrorCallback callback function) but the strange thing is that the value of handle->ErrorCode is zero! So, an error but no error code. I think there ...

change pin status UART to GPIO

Posted on July 05, 2018 at 08:10Hi everyone, in my system (freertos based) i need some low pulse before sending uart datas. So i must change tx pin to gpio and send low pulse along appx. 100uS and after that i must rechange it to uart fastly. How ca...

Resolved! Dose cubemx support stm32h7 using other phy ic

Posted on July 01, 2018 at 15:32Dear all:     Dose cubemx support stm32h7 using other phy ic, not only using lan8742, like stm32f4. The first pic is cubemx support stm32h7,the second pic is cubemx support stm32f4,the different between two pics is th...

0690X0000060C7rQAE.png 0690X0000060C7wQAE.png
Yi Zhou by Associate III
  • 1466 Views
  • 2 replies
  • 0 kudos

STM32H7 SCB_CleanInvalidateDCache ERROR

Posted on April 23, 2018 at 17:03I'm using CubeMx to generate the basic configuration for NUCLEO-H743ZI board;Default settings are used, FREERTOS and LWIP flags are enabled sys timebase source set to TIM1as suggested by CubeMx. Project files are gen...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.