STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Low Level SPI transaction on STM32F439z

I've been messing with the LL drivers for SPI and have run into some confusion.I have HCLK set to 100 Mhz and PCLK1 set to 25 Mhz.I set up the bus using the code generated from STM32cubeMX:static void MX_SPI1_Init(void) {   /* USER CODE BEGIN SPI1_...

0690X0000087dQiQAI.jpg 0690X0000087dQdQAI.jpg 0690X0000087dQnQAI.jpg
CMott by Associate
  • 5068 Views
  • 7 replies
  • 0 kudos

STM32F103 boot loader question

Occasionally I get a crash - I think when stack meets heap in certain circumstances but I'm still working on that and it's not the issue I'm asking about.The problem is that when the processor crashes I use the boot loader to reload another code buil...

MikeDB by Lead
  • 757 Views
  • 0 replies
  • 0 kudos

in STM32F373 SDADC example for RTD measurement and I am getting huge noise in raw ADC and RTD temperature variation after configuring other peripherals like TSC and SPI for LCD.

I have used SDADC RTD temperature measurement example from \STM32Cube\Repository\STM32Cube_FW_F3_V1.10.0\Projects\STM32373C_EVAL\Examples\SDADC\SDADC_TempMeasurementwith the same micro STM32F373 and I am getting huge noise in raw ADC and RTD temperat...

Communication UART

Good morning,HAL_UART_Transmit(&huart2,myRxData,11,10);HAL_UART_Receive(&huart2,myRxData,11,100);My question is: only to make a test of sending and receiving data is enough to use the previous functions and make the connection of the pins tx with rx ...

lmeli by Associate II
  • 4150 Views
  • 9 replies
  • 0 kudos

Resolved! Use of UART HAL Drivers

Hello,I'm designing an application where a PCB with STM32F031C6 has to receive a minimum of 5 bytes via an half-duplex communication. Transmission is delimited by special character, ASCII is used. Ideally, the transmission would be composed by 3 data...

MFran.10 by Associate II
  • 2991 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.