STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Update only one section with code/functions

Hello,I was wondering if it was allways necassary to implement a bootloader and load the entire app to flash. Would it be possible to place some frequently updated functions in an own section (with variables stored in own section in Ram) and only upd...

machinist by Associate III
  • 1526 Views
  • 3 replies
  • 0 kudos

STM32L433 doesn't generate the UART_IT_IDLE Interrupt

Hello, everyoneI have an STM32L433 that must communicate with other device via UART.When I activate xfer with commands:__HAL_UART_ENABLE_IT(uartHandle, UART_IT_IDLE); HAL_UART_Receive_DMA(uartHandle, &rxBuffer[0], rxBufferSize);I expect that when o...

Uhv by Associate II
  • 831 Views
  • 0 replies
  • 1 kudos

Problem with USB CDC on STM32F4-Discovery

Hello.I'm working with STM32F4-Discovery. I use USB CDC VCP for transmit data from ADC to PC and receive command from PC to change timer period. Program is written with HAL drivers, with help of CubeMX. Problem is with receiving command, because some...

leonsk by Associate II
  • 847 Views
  • 0 replies
  • 0 kudos

Resolved! STM32G071 UCPD library bug or my bad?

Hello there, I have a custom board with STM32G071CB for USB Type C PD Source, dual port, RTOS, configured with CubeMX 5.3.0, after writing code on usbpd_dpm_user.c and start debugging, I suspected there are 2+1 strange behavior so I hope somebody can...

JChau by Associate II
  • 5583 Views
  • 12 replies
  • 0 kudos

Resolved! CDC function added but no any com port shown

I want to add CDC function. I use the STM32F103RB NUCLEO to add this function. But when I running my application, and insert USB to PC, no COM port shown in PC. I generate the code from cube and I don't know where is the problem. I test WIN10 and WIN...

0690X000009Z0poQAC.png 0690X000009Z0peQAC.jpg

USB PID and USB VID usage

Hello! We would like to know if it is possible to use your USB VID and default USB PID from the USB CDC library source code in commercial products? And also learn, if necessary, about the purchase of USB PID on our product and what you need to get it...

dmkuzmin by Associate
  • 1496 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.