2019-07-23 9:13 AM
Hi Community, my application use FreeRTOS work fine when i did not use PWR_EnterSTANDBYMode. The problem is the program did not run some function like skip function after wake up, For instance: usart2_init, delay.. when I debug and put the break point at that function. The program work properly. Please help me.
I use StdPeriph_Driver library and use stm32f1 before, I am new in using stm32L1xx
2019-07-23 9:52 AM
You have to turn on the clocks again
STM32L1xx_StdPeriph_Lib_V1.3.1\Project\STM32L1xx_StdPeriph_Examples\PWR\STOP\main.c
...
/* Enable Wakeup Counter */
RTC_WakeUpCmd(ENABLE);
/* Enter Stop Mode */
PWR_EnterSTOPMode(PWR_Regulator_LowPower, PWR_STOPEntry_WFI);
// Sometime later... (in Spongebob announcer voice)
/* Disable Wakeup Counter */
RTC_WakeUpCmd(DISABLE);
/* After wake-up from STOP reconfigure the system clock */
/* Enable HSE */
RCC_HSEConfig(RCC_HSE_ON);
/* Wait till HSE is ready */
while (RCC_GetFlagStatus(RCC_FLAG_HSERDY) == RESET)
{}
/* Enable PLL */
RCC_PLLCmd(ENABLE);
/* Wait till PLL is ready */
while (RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET)
{}
/* Select PLL as system clock source */
RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);
/* Wait till PLL is used as system clock source */
while (RCC_GetSYSCLKSource() != 0x0C)
{}
2019-07-24 9:01 AM
I use PWR_EnterSTANDBYMode not PWR_EnterSTOPMode, I test and find out that my stm32l is reset on wake up(run from begin app). I also initial clock to 32Mhz after wake up. I also try insert this code but has not change. Thanks for reply
/* Disable Wakeup Counter */
RTC_WakeUpCmd(DISABLE);This is my function to initial RCC.
ErrorStatus HSEStartUpStatus;
/* SYSCLK, HCLK, PCLK2 and PCLK1 configuration -----------------------------*/
/* RCC system reset(for debug purpose) */
RCC_DeInit();
/* Enable HSE */
RCC_HSEConfig(RCC_HSE_ON);
/* Wait till HSE is ready */
HSEStartUpStatus = RCC_WaitForHSEStartUp();
if (HSEStartUpStatus == SUCCESS)
{
/* Enable 64-bit access */
FLASH->ACR |= FLASH_ACR_ACC64;
/* Enable Prefetch Buffer */
FLASH->ACR |= FLASH_ACR_PRFTEN;
/* Flash 1 wait state */
FLASH->ACR |= FLASH_ACR_LATENCY;
/* Power enable */
RCC->APB1ENR |= RCC_APB1ENR_PWREN;
/* Select the Voltage Range 1 (1.8 V) */
PWR->CR = PWR_CR_VOS_0;
/* Wait Until the Voltage Regulator is ready */
while((PWR->CSR & PWR_CSR_VOSF) != RESET)
{
}
/* HCLK = SYSCLK /1*/
RCC->CFGR |= (uint32_t)RCC_CFGR_HPRE_DIV1;
/* PCLK2 = HCLK /1*/
RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE2_DIV1;
/* PCLK1 = HCLK /1*/
RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE1_DIV1;
/* PLL configuration */
RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_PLLSRC | RCC_CFGR_PLLMUL |
RCC_CFGR_PLLDIV));
RCC->CFGR |= (uint32_t)(RCC_CFGR_PLLSRC_HSE | RCC_CFGR_PLLMUL12 | RCC_CFGR_PLLDIV3);
/* Enable PLL */
RCC->CR |= RCC_CR_PLLON;
/* Wait till PLL is ready */
while((RCC->CR & RCC_CR_PLLRDY) == 0)
{
}
/* Select PLL as system clock source */
RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_SW));
RCC->CFGR |= (uint32_t)RCC_CFGR_SW_PLL;
/* Wait till PLL is used as system clock source */
while ((RCC->CFGR & (uint32_t)RCC_CFGR_SWS) != (uint32_t)RCC_CFGR_SWS_PLL)
{
}
}
2019-07-25 8:06 AM
The problem is solved. Nothing wrong here. My board connect to a sensor and the sensor not work properly. That is really make me confuse when I try to debug. I just though the debug did not work properly, although I initial core clock to 32Mhz.(ps: I even think about has error in IDE.)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.