STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can't blink LED with HAL

Hey all,I have a 32F469IDISCOVERY BOARD that I'm trying to use with CubeIDE, and all I'm trying to do right now is blink an LED with the HAL.Starting from a new project, all periherals are initialized with their default settings.In the User Code 3 lo...

AJaro.2 by Associate II
  • 1659 Views
  • 2 replies
  • 0 kudos

Problems with using GPIOs

Hello ST CommunityI'm currently trying to understand Cortex MCUs and thought about going to LL instead o fusing the HAL.Since I've just started with the STM32G071RB, I'm having trouble configuring the Pin A5 as an output and setting it high.My code l...

Using USB OTG_HS in STM32F730R8

STM32F730R8 has embedded USB OTG_HS peripheral and internal FS OTG PHY support. What are the register settings required to run USB FS on the OTG_HS peripheral? What should be the system clock settings?

SVark.15 by Associate
  • 1604 Views
  • 2 replies
  • 0 kudos

STM32F723 USB Device MSC with internal flash

Hi!I am using stm32f723 to implement usb device mass storage.I try to mass storage using an internal flash, but I get a message that the formatting is not complete.I have developed it by referring to the link below, and I have confirmed the same valu...

SKoh.12 by Associate II
  • 3362 Views
  • 4 replies
  • 0 kudos

STM32L476RG FreeRTOS multithread issue

Hi Experts,I am using STM32L476G MPU, (which sensortile board) and used the following SDK & sensortile BLE example.~\STSW-STLKT01_V1.3.1\Projects\SensorTile\Applications\BLE_SampleAppAdded FreeRTOS support for multithread in my BLE example.~\STSW-STL...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.