STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to restart into bootloader (with DFU).

typedef void resetvec(void);       void cmd_jbl(BaseSequentialStream *chp, int argc, char **argv) // reboot to bootloader   {    unsigned int t;        (void)argc;     (void)argv;    (void)chp;    resetvec *fun;         fun = ((uint32_t *)0x1fffc800)...

UCB CVP won't work in STM32F412RG

I'm struggling already many days getting the most simple VCP functionality working in my application.I tried implementing the UM1021 usb OTG lib provide as extension on the STD peripheral library from ST, but without succes. After that I tried the s...

SMaes.3 by Associate
  • 780 Views
  • 0 replies
  • 0 kudos

Hello! I'm testing FatFS on my evaluation board and is working only for a 2gb sd card. I'm using the example from the Cube repository. Can anyone help me?

I'm need to use a microSD card on my new project, so I decided to test in my evaluation boards. I have a STM32373C-EVAL and a STM3210C-EVAL boards. For the tests I used 2Gb, 4Gb, 8Gb and 16Gb sd cards. Now came the problem, on the STM32373C-EVAL only...

What is the difference between 'USB CDC' and 'USB HID'?

I'm using STM32F072VB.​I want to communicate with 'USB' instead of 'Serial'.Should i use ​'USB CDC(VCP)'? or Should i use 'USB HID'?I ​created a 'USB HID' test code with CubeMX and checked it. ( Reference Image1)​​<Image1>​Can i do 'download communic...

0690X0000098Qi7QAE.png
LHAEU by Associate
  • 1623 Views
  • 0 replies
  • 0 kudos

F103 USB HID works when not debugging (swd)

Hello,​I'm trying a really simple HID mouse-moving example (https://notes.iopush.net/stm32-custom-usb-hid-step-by-step-2/) and if I connect my bluepill via usb to the computer (macOS), as expected, it connects and the mousecursor slowly drifts to the...

RBoer by Associate II
  • 2662 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.