STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I cannot see the status of the registers DFSDM1_Filter2 and DFSDM1_Filter3 in register view STM32l496ZG.

When you configure DFSDM faced with the problem that I can't see the status registers a custom filter, due to incorrect file STM32L4x6.svd because the register addresses according to this file do not match those described in the Datasheet and in the ...

Dumpler by Associate
  • 1370 Views
  • 3 replies
  • 0 kudos

VBUS sensing not working at Stop Mode

I'm used mcu stm32l476vg.I'll have to low power mode.It is in low power mode using the following API.HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI);But although it is in low power mode, it does not return by USB insertion.I ask for yo...

KMats.2 by Associate
  • 1025 Views
  • 1 replies
  • 0 kudos

Enabling fault handlers

Hi. I've run into an interesting situation and hopefully someone can give me an answer, or at least a suggestion.We've got a product in development. In the last few months we've seen a couple of them (2 or 3, that we know of) freeze and become unresp...

LThal by Associate III
  • 2115 Views
  • 2 replies
  • 0 kudos

Logico convert

hi I have an encoder that has channel A channel B 5 volt output only and I wonder if it is possible to read gpio interrupt with a cortex m4 since it works at 3.3 volts? Do you need a logic level converter, some resistor or read it anyway?

SDall by Associate II
  • 1119 Views
  • 2 replies
  • 0 kudos

STM32CDC Windows and OOB data?

I have a STM32F303 acting as a serial port to an industrial control system, but I need a reliable way to set a byte for out-of-band data (I need to set "termination resistor On/Off, Drive Strength, etc -- I'm using the "comm port" for the serial data...

TJohn.14 by Associate II
  • 2465 Views
  • 4 replies
  • 0 kudos

Polling ADC on STM32F777IIK

I'm having problems getting an ADC value from the STM32F777IIK chip we have embedded in one of our boards.I have used a digital GPIO application and have confirmed that the ADC pin (PC0) is connected from the chip to the headers that is good.I have u...

Nevyn by Associate II
  • 3202 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.