STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

F446ZE - Keyboard and mouse USB host!

Hey,Doing some research on STM32F446ZE and i have successfully made both USB ports to work with a HID device. HS as a FS with my own USB female, and ofcourse with the onboard usb-in.My goal is to use the board as a host for both keyboard and mouse si...

jomoi by Associate II
  • 1864 Views
  • 3 replies
  • 1 kudos

Multi-channel SDADC on STM32F373 using HAL

This question was asked but it is now closed , so i want to ask again If some one can share code of how to do sdadc3 for multichannel viaDMA |ISR | interrupts | preferred DMAAll code example shows how to work with single channel.The reason ...

EA50 by Associate
  • 1418 Views
  • 1 replies
  • 0 kudos

SMBUS Example code

I am using STM32F779NI for my project. The end device works on SMBUS. Does using I2C HAL for driver development instead of SMBUS HAL will work??If not, are there any example code for SMBUS, share a link if there is any?

A3 by Associate III
  • 994 Views
  • 0 replies
  • 0 kudos

Problem Implementing Fatfs on spi flash 1MB . hi i am trying to port Fatfs generated from cube mx on to my spi flash on stm32 board.

when creating and opening a file i get error and it exits what could be the problem below i have shared the code .////////////////////////////////////main.c///////////////////////////////////////////if( FATFS_LinkDriver(&USER_Driver, USERPath)== 0)...

svii by Associate III
  • 2159 Views
  • 4 replies
  • 0 kudos

Hi all, Does anybody has any idea what is "The parameter is incorrect" error. I am using nucleo f429zi board. the problem occurs when i am using ethernet with the USB. The PC can detect the virtual com port but gives error when you try to connect to it.

If i disable the ethernet (comment the MX_LWIP_INIT function) the USB works fine. I am only using the cube MX generated code no fancy thing at all. The next thing I tried to do was to do the same thing on STM3249zi eval board but I was surprised to s...

Mr ZEE by Associate II
  • 715 Views
  • 0 replies
  • 0 kudos

I am testing the boot mode of STM32G070 with Nucleo-G070RB board, using an IAR I-iet emulator. Thanks.

I try to use UART to download firmware to the board with STM32CubeProgrammer, UART 1 was connected to the PC. I added the following code trying to set the MCU to boot mode, but after run this code, my I-jet emulator stop working, cannot talk to the C...

CChen.16 by Associate II
  • 1589 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.