2018-11-20 5:53 AM
Hello there!
I'm working with Nucleo-H743ZI and LwIP stack, generated by CubeMX, and I've enabled HTTPD routine for a simple webserver (further I'll add some POST commands). Everything works ok if LWIP_HTTPD_DYNAMIC_HEADERS is disabled. When enabled (removing headers from fsdata), the page doesn't load at all. After some debug process, I noticed that "http_write" method from "http_send_headers" only works if "apiflags = TCP_WRITE_FLAG_COPY". A "0" value or even "TCP_WRITE_FLAG_MORE" doesn't work (no packages on Wireshark). The problem using copy flag is the page became very slow and instable (on Wireshark, each header has a "PSH" flag).
Is anyone there facing the same problem?
Thanks a lot!
2019-11-12 8:29 AM
Hi, I have the same problem.
Did you find a solution?
2019-11-12 1:40 PM
Hello, I'm sorry not posting a solution before...
I'm using TCP_WRITE_FLAG_COPY for all tcp_write operation and increasing MEM_SIZE defined value solved the "slow and instable" issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.