2019-11-12 12:37 AM
If i disable the ethernet (comment the MX_LWIP_INIT function) the USB works fine. I am only using the cube MX generated code no fancy thing at all. The next thing I tried to do was to do the same thing on STM3249zi eval board but I was surprised to see that USB was working fine with the ethernet, no errors at all.
The question is that is it something to do with the hardware?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.