STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 alternate function mapping confusion

It is very confusing to me how pin multiplexer is explained in the datasheet, it doesnt help the matter when using .SVD file in the debugger as it is even more confusing.Lets start with the SVD file. In the debugger I can see AFRL showing AFRL0-AFRL7...

Gossamer by Associate II
  • 2452 Views
  • 3 replies
  • 0 kudos

STM32F769 IsoINIncomplete callback gets called multiple times in a row but OTG_DAINT register has the value 0x00000000. What can be the reason?

Hi, I am working with the STM32F769i-disco board and develop an usb audio 2.0 device (a microphone array). When I start a recording application on the host pc, the IsoINIncomplete callback gets called multiple times in a row but the OTG_DAINT registe...

MGuen.1 by Associate
  • 1092 Views
  • 0 replies
  • 0 kudos

Regarding FreeRTOS

Hi ST Team,Hope all you are Well !!!!I have a STM32F030 Nucelo-64 EV BOARD. I wanted to work on FreeRTOS on this Board. Can you help me how can i proceed on this.

PKuma.6 by Associate II
  • 2027 Views
  • 3 replies
  • 0 kudos

Resolved! F042K6 - stuck in CAN receive interrupt

Hello,I am trying to set up CAN communication on my F042K6 using the HAL library. I have followed the stm guide (attached). I got most of the functionality working, however if i try to use the Rx interrupt using "void HAL_CAN_RxFifo0MsgPendingCallbac...

retro by Associate III
  • 8896 Views
  • 12 replies
  • 0 kudos

Resolved! STM32F411CEU6 "Black Pill" USB virtual COM port code not working, but working on STM32F4 discovery

Hello,I'm using STMCubeIDE, with firmware version: STM32Cube FW_F4 V1.25.0I am trying to implement a USB virtual COM port. My code is working on the STM32F4 discovery board. I then created a new project for the STM32F411CEU6 "Black Pill", but the U...

Gbeau.1 by Associate
  • 8052 Views
  • 1 replies
  • 0 kudos

STM32F76XXX Bootloader Activation

Hi! I'm new to the STM32F76, and I'm attempting to flash the MCU through either a serial/USART connection or USB (DFU mode). I have been unsuccessful and would appreciate any advice.Here's what I've tried:* I've read through AN2606 and have gathered ...

BB.2 by Associate
  • 1516 Views
  • 2 replies
  • 0 kudos

ADC_CHANNEL_10: Wrong query during code generation

I use STM32CubeMX (5.6.1) with a STM32F373. When creating the hardware initialization with CubeMX there is an error in the "stm32F3xx_hal_adc_ex.c" file. When querying the channel used, an equals sign is missing for both "sConfig" and "sConfigInjecte...

0693W000001rjdrQAA.png 0693W000001rje6QAA.png
CWres by Associate
  • 731 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.