STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unexpected restart, NUCLEO-L432KC

Hello,I want to use a NUCLEO-L432KC as an interface card on a computer.The L432KC reboots when it is plugged into the USB port of my computer in Windows 10.These restarts occur randomly after a few minutes.These restarts also occur if I supply it wit...

MBASL.1 by Associate
  • 1064 Views
  • 1 replies
  • 0 kudos

FATfs library for QSPI flash

is there any library available to handle FATfs file management system over QSPI flash, I've checked it is available for SD card, may be some part of it can be used but if its available for QSPI flash which directly can be used.

AShel.1 by Associate III
  • 3678 Views
  • 8 replies
  • 0 kudos

Resolved! SPI slave and SSI bit

Hi there,Lets say my device is configured as an SPI slave device with a software NSS pin. The STM32 HAL API doesn't use the SSI bit from CR1 register at all. I was wondering, what actually happens to the SPI peripheral when I manually set or clear th...

NUCLEO-L552ZE-Q PD Issue

I've a problem to setup the NUCLEO-L552ZE-Q as PD Sink.The debugger always disconnect at the following line (void HardFault_Handler(void)):CHECK_CAD_FUNCTION_CALL(USBPD_CAD_Init(USBPD_PORT_0, (USBPD_CAD_Callbacks *)&CAD_cbs, (USBPD_SettingsTypeDef *)...

TG..1 by Associate II
  • 3320 Views
  • 5 replies
  • 0 kudos

UART Rx Interrupt triggered, but state is READY, when it should be BUSY, causing Rx Data to not be returned.

STM32H743Using USART3 in Asynchronous mode with interrupt. The hope is to use this with FreeRTOS+CLII am able to Tx as expected. Rx will trigger the interrupt, but the RX State is READY when it should be BUSY. This causes the value to not be saved, a...

PLane.1 by Associate II
  • 2178 Views
  • 1 replies
  • 0 kudos

FOTA using UART bluetooth

I am using an STM32F302CB MCU, I intend to program my device remotely via a mobile app connected with the embedded system through a BT( UART connected).What I understood:-1.) The ST bootloader can be used to flash the MCU by sending some commands to ...

Svish.2 by Associate II
  • 3739 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.