2020-06-29 10:12 AM
Hi! I'm new to the STM32F76, and I'm attempting to flash the MCU through either a serial/USART connection or USB (DFU mode). I have been unsuccessful and would appreciate any advice.
Here's what I've tried:
* I've read through AN2606 and have gathered that in order to activate the bootloader, I need to follow pattern 9. For example: nDBANK(bit) = 1, Boot(pin) = 1 and BOOT_ADD1(optionbyte) = 0x0040; please correct me if I'm wrong.
* Using the ST-Link utility, I have verified that nDBANK is checked and that BOOT_ADD1 = 0x0040
* I have a jumper between BOOT0 and VCC
What am I missing here? It seems like flashing the STM32F4 is pretty trivial; I've found loads of resources online for that, but there's not much on flashing the STM32F7x.
Is it possible that I somehow don't have the proper bootloader? I was under the impression that this was flashed by STM and was present on the MCU by default. Do I need some sort of special flags set in my firmware? Is there another pin that I need to be pulling? Any help is greatly appreciated
2020-06-29 11:26 AM
You can view the ROM code via JTAG/SWD or your own code.
Thing to watch on the boot loader is ANY signals on the interfaces it is looking for interaction on.
For example don't connect a GPS receiver to any UART it is monitoring, as these start and send periodic data at startup
2020-06-29 11:36 AM
Thanks for the reply! I'll check that out
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.