STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LWIP and SNTP

Hi,I am looking at:STM32Cube_FW_H7_V1.7.0\Middlewares\Third_Party\LwIP\src\apps\sntpHow is it supposed to be used ?What I did:void SNTP_Thread(void const *arg) { sntp_setoperatingmode(SNTP_OPMODE_POLL); sntp_setserver(0, &sntp_addr); printh(" (%d)...

Could you share a USB OTG example?

I am looking to implement USB OTG on a STM32H757 evaluation board. From my reading, it has been made clear that ST does not provide library support for USB OTG and it does not currently have any examples available. I am not looking for an incredibly ...

YReda.1 by Associate
  • 1240 Views
  • 1 replies
  • 1 kudos

Bootloader stucks in UART initialisation (waiting for USART_ISR_REACK flag) after aplication clocks it from PLL

MCU: STM32H743 revision YI am preparing firmware update. Update works by storing firmware in external flash, setting a flag in backup RAM, printing goodbye message via UART and executing NVIC_SystemReset(). Then bootloader sees the flag in backup RAM...

JSima.1 by Associate
  • 1622 Views
  • 2 replies
  • 0 kudos

STM32F4 LL RTC and RCC are a total disaster

Hi all,I would like to point out a total disaster if you are using the LL library for RCC and RTC for the F4 series family. Let me start with the system clock config, which falls under RCC. Why the hell is there a default wipe of backup domain regist...

MKsen.1 by Associate II
  • 1198 Views
  • 0 replies
  • 2 kudos

I am using X-CUBE-AWS packages with p-l496g-cell01 development board to send my sensor data on AWS it works fine buy during sometime code will stick and it generates an error

I am using X-CUBE-AWS packages with p-l496g-cell01 development board to send my sensor data on AWS it works fine buy during sometime code will stick and it generates an errorI also enable "isAutoReconnectEnabled" flag but it genrate error likeERROR: ...

pragnesh by Associate III
  • 1259 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.