2020-07-22 12:42 PM
I've been sucessfully using the SD card example in the CubeF7 files, but I can't understand where the SPI connections are set up, and if I was to choose SDIO instead, where would I do that?
It seems to just magically know I've connected it to the SPIA port on the nucleo board, without any of the lengthy initialisation you normally see in the main.c file.
Thanks!
2020-07-22 1:42 PM
The NUCLEO / ADAFRUIT stuff is hidden in the BSP code
STM32Cube_FW_F7_V1.16.0\Drivers\BSP\STM32F7xx_Nucleo_144\stm32f7xx_nucleo_144.h
/*############################### SPI_A #######################################*/
#ifdef HAL_SPI_MODULE_ENABLED
#define NUCLEO_SPIx SPI1
#define NUCLEO_SPIx_CLK_ENABLE() __HAL_RCC_SPI1_CLK_ENABLE()
#define NUCLEO_SPIx_SCK_AF GPIO_AF5_SPI1
#define NUCLEO_SPIx_SCK_GPIO_PORT GPIOA
#define NUCLEO_SPIx_SCK_PIN GPIO_PIN_5
#define NUCLEO_SPIx_SCK_GPIO_CLK_ENABLE() __HAL_RCC_GPIOA_CLK_ENABLE()
#define NUCLEO_SPIx_SCK_GPIO_CLK_DISABLE() __HAL_RCC_GPIOA_CLK_DISABLE()
#define NUCLEO_SPIx_MISO_MOSI_AF GPIO_AF5_SPI1
#define NUCLEO_SPIx_MISO_MOSI_GPIO_PORT GPIOA
#define NUCLEO_SPIx_MISO_MOSI_GPIO_CLK_ENABLE() __HAL_RCC_GPIOA_CLK_ENABLE()
#define NUCLEO_SPIx_MISO_MOSI_GPIO_CLK_DISABLE() __HAL_RCC_GPIOA_CLK_DISABLE()
#define NUCLEO_SPIx_MISO_PIN GPIO_PIN_6
#define NUCLEO_SPIx_MOSI_PIN GPIO_PIN_7
...
/**
* @brief SD Control Lines management
*/
#define SD_CS_LOW() HAL_GPIO_WritePin(SD_CS_GPIO_PORT, SD_CS_PIN, GPIO_PIN_RESET)
#define SD_CS_HIGH() HAL_GPIO_WritePin(SD_CS_GPIO_PORT, SD_CS_PIN, GPIO_PIN_SET)
...
/**
* @brief SD Control Interface pins (shield D4)
*/
#define SD_CS_PIN GPIO_PIN_14
#define SD_CS_GPIO_PORT GPIOF
#define SD_CS_GPIO_CLK_ENABLE() __HAL_RCC_GPIOF_CLK_ENABLE()
#define SD_CS_GPIO_CLK_DISABLE() __HAL_RCC_GPIOF_CLK_DISABLE()
Different example? Be specific..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.