2020-07-17 12:02 AM
I try use the boot loader command set.
I follow the AN3155 datasheet to use , but i meet a trouble, i can't write bytes over 4 bytes. below is my set step
but if I want to write more byte or one bin file , then device all response 1F(NACK)
example :
host-> 0c 00 04 00 20 a9 8b 00 00 03 8e 00 00 00 00 /device ->1F
send 128 bytes host-> 80 00 04 00 20..............80 00 00 00 00 /device->1F
Could you talk me where is error? thank you
2020-07-17 6:04 AM
> 04 00 04 00 20 00 20
This writes 5 bytes, not 4.
> 0c 00 04 00 20 a9 8b 00 00 03 8e 00 00 00 00
This writes 13 bytes and the checksum is wrong.
2020-07-21 8:11 PM
Please tell me how to cal the checksum?? and the data string checksum is ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.