2017-10-10 9:54 AM
I wish to have an example program to flash my stm32F7 /stm32H7 mcu to flash via ethernet or over the network.
Anybody has any such try outs?
#stm32h7 #ethernet #flashing #ethernet-stm32f72017-10-10 10:29 AM
I would imagine the existing IAP examples should demonstrate the technical requirements and be generally portable.
2017-10-17 6:27 AM
Hi
PARAKKAL.SIJOMON
,as
Turvey.Clive
, I would recommend to start withhttp://www.st.com/en/embedded-software/stm32cubef7.html
examples.In
http://www.st.com/resource/en/application_note/dm00210pdf
, if you search for IAP, you will find the various examples of In Application Programming provided. One of them,LwIP_IAP, is for IAP over Ethernet (p. 41 of AN4731), and available in the folder:STM32Cube_FW_F7_V1.8.0\Projects\STM32F769I_EVAL\Applications\LwIP\LwIP_IAP
Extract from readme.txt:
This application guides STM32Cube HAL API users to run In-Application Programming (IAP) over Ethernet.
Two IAP options are provided:
- IAP using TFTP (Trivial File Transfer Protocol) - IAP using HTTP (Hypertext Transfer Protocol)Best regards,
Cédric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.