2017-10-17 6:54 AM
STM32_USB-FS-Device_Lib_V4.1.0
file :usb_core.c
funciton name: RESULT Standard_ClearFeature(void)
code :
if (wIndex0 & 0x80)
{
/* IN endpoint */
if (_GetTxStallStatus(Related_Endpoint ))
{
ClearDTOG_TX(Related_Endpoint);
SetEPTxStatus(Related_Endpoint, EP_TX_VALID);
}
}
else
{
/* OUT endpoint */
if (_GetRxStallStatus(Related_Endpoint))
{
if (Related_Endpoint == ENDP0)
{
/* After clear the STALL, enable the default endpoint receiver */
SetEPRxCount(Related_Endpoint, Device_Property.MaxPacketSize);
_SetEPRxStatus(Related_Endpoint, EP_RX_VALID);
}
else
{
ClearDTOG_RX(Related_Endpoint);
_SetEPRxStatus(Related_Endpoint, EP_RX_VALID);
}
}
}
question: i saw that status of IN endpint was set to VALID(EP_TX_VALID) after recover from HALT;
i wonder why we don't set the status to NAK;
The USB spec doesn't specify how to leave the endpoints after a halt is cleared.
but for an interrupt IN endpoint such as a HID device,at that point when the endpoint recover from halt status,the device will send an packet with uncertain data to the host,since the host automatically query the device by IN token in a determined interval constantly,and it can be quite possible for the packet buffer contains uncertain data at that point;
possible advice: just set the status to NAK,firmware could set it to VALID if necessary data get ready to transfer to host later.
Regards,
uzslm
#usb-clearfeature-seteptxstatusWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.