2012-04-12 1:26 AM
To integrate firmware update functionality into a custom c♯ application I start to use ST Dfuse dll from c♯. I managed to enumerate and identify the device (UM0392 - 3.1 and 3.2) but now get stucked while trying to erase the device. Out of the manual:
DWORD OperationCode; PDWORD pNbAlternates; PMAPPING pMapping; PHANDLE pHandle; // Programming the operation contex lstrcpy(Context.szDevLink, DFUName); Context.DfuGUID=GUID_DFU; Context.AppGUID=GUID_APP; Context.Operation=OPERATION_ERASE; Context.bDontSendFFTransfersForUpgrade= TRUE; STDFUPRT_CreateMappingFromDevice((LPSTR)(LPCSTR)DFUName,&pMapping, &NbAlternates); STDFUFILES_CreateImageFromMapping(pHandle, pMapping); STDFUFILES_FilterImageForOperation(hImage, m_pMapping+TargetSel, OPERATION_ERASE, FALSE); Context.hImage=hImage; if( STDFUPRT_LaunchOperation(&Context, &OperationCode) != STDFUPRT_NOERROR) { Printf(�Erase error�); } The call of STDFUPRT_LaunchOperation() does always return a STDFUPRT_BADPARAMETER error. Is there a way to get some more information about this error? Which parameter is bad? The first parameter in LaunchOperation() is a pointer to the struct DFUThreadContext. I rebuilt this struct in c♯ using the information given in UM0384.pdf chapter 4.3.4. My UM0384 is revision 1 - June 2007 - wonder if that user manual is still up-to-date?!? I did not find UM0384 on the webpage (my copy is out of the package UM0412.zip). Does anyone have a newer one? Thanks in advance for any help #st-dfu #st-dfuse #dfuse2012-06-08 5:07 AM
Finally I realized how to handle the mapping-pointer stuff. I used a simple, unmanaged struct for the mapping (because I need to set pointers to that struct). Here my code:
[StructLayout(LayoutKind.Explicit, CharSet = CharSet.Auto)] public unsafe struct UmMAPPING { [FieldOffset(0)] public byte nAlternate; [FieldOffset(1)] public char Name; [FieldOffset(261)] public UInt32 NbSectors; [FieldOffset(265)] public MAPPINGSECTOR* pSectors; } UmMAPPING UmMapping; UmMAPPING* pUmMapping = null; error_code = STDFUPRT_CreateMappingFromDevice(Context.szDevLink, ref pUmMapping, ref pNbAlternates); UmMapping = *pUmMapping; error_code = STDFUFILES_CreateImageFromMapping(ref pHandle, ref UmMapping); ... You will find the first two ascii letters in the property Name (0x49 = ''I'', 0x6e = ''n''). For my device the name of the first map is ''Internal Flash''. I used STDFU Tester to check that. However it doesn't do anything. No exceptions/errors but also no erasing. I'm wondering if the example from ST is correct (complete) or if perhaps another function call is missing ....2012-06-08 7:20 AM
Struct DFUThreadContext seems to be wrong and therefore STDFUPRT_LaunchOperation() doesn't do anything. I did a simple test with the following code to check if the values in DFUThreadContext are placed in the correct order.
List<UInt32> test = new List<UInt32>(); test.Add((UInt32)(UInt32*)&Context.DFUGUID); test.Add((UInt32)(UInt32*)&Context.APPGUID); test.Add((UInt32)(UInt32*)&Context.Operation); test.Add((UInt32)(UInt32*)&Context.bDontSendFFTransfersForUpgrade); test.Add((UInt32)(UInt32*)&Context.hImage); //test.Add((UInt32)(UInt32*)&Context.szDevLink); test.Add((UInt32)(UInt32*)&Context.dwTag); test.Add((UInt32)(UInt32*)&Context.percent); test.Add((UInt32)(UInt32*)&Context.wTransferSize); I expected the pointeraddresses increase constantly but they don't! It does not place one value after the other like in the definition of the struct. So I defined the struct with LayoutKind.Explicit and checked again - now they are in a row. With this new struct STDFUPRT_LaunchOperation() returns error 0x12345008. There is no description of this error in UM0384. Does anyone know something about this error??2012-06-08 7:27 AM
Hi Jonas!
first of all thanks for sharing the code! it really helps a lot, I am having a little bit of trouble fixing the signatures for the dll import right now I have this. [DllImport(''STDFUFILES.dll'', EntryPoint = ''STDFUFILES_CreateImageFromMapping'', CharSet = CharSet.Auto)] public static extern UInt32 STDFUFILES_CreateImageFromMapping(ref IntPtr handle, ref STDFUPRT.UmMAPPING* puMapping);but is not compiling, I am not sure how to place the pointer parameter in the signature. I was wondering if I could see yours. Thanks. Marco.2012-06-08 7:37 AM
Remove *. It's already a reference because of ''ref'' :)
Ps: In c++ source code I found those lines: #define STDFUPRT_ERROR_OFFSET (0x12340000+0x5000) #define STDFUPRT_BADPARAMETER (STDFUPRT_ERROR_OFFSET+0x0008) obviously error 0x12345008 says there is a bad parameter. hmmm.. doesn't help me a lot. Two months ago as I started this discussion I had the same error - annoying.2012-06-08 8:05 AM
so you declaration looks like this?
[DllImport(''STDFUPRT.dll'', EntryPoint = ''STDFUPRT_CreateMappingFromDevice'', CharSet = CharSet.Auto)]public static extern UInt32 STDFUPRT_CreateMappingFromDevice([MarshalAs(UnmanagedType.LPStr)]string DFUNAME, ref STDFUPRT.UmMAPPING puMapping, ref UInt32 pNbAlternates);I am super confused with this, because when you call your function you pass the pointer.''STDFUPRT_CreateMappingFromDevice(Context.szDevLink, ref pUmMapping, ref pNbAlternates);''
sorry if these are too elemental questions, I don't have too much experience with this.thanks in advance.2012-06-08 8:23 AM
you probably mixed up the two functions. they need different parameter:
CreateImageFromMapping: it demands a reference so put ref but no * -> ref STDFUPRT.UmMAPPING puMapping CreateMappingFromDevice: it demands a reference to a reference so put both * and ref and use unsafe -> ref STDFUPRT.UmMAPPING* puMapping2012-06-08 8:42 AM
ugh, sorry man you are totally right.
Thanks! I'll let you know If I have any progress by the en of the day ... lol forum time seems to be european time ... here is just 10:40 AM ... Have a good Weekend!2012-06-08 8:52 AM
There must be an error in UM0384 table 13 DFUThreadContext class.
Field Operation has a size of 4. If I change this I do not receive the error above but an AccessViolationException. There are probably even more mistakes in this manual. Could anyone from ST PLEASE verify this??? PS: Good luck marco cheers, till Monday2012-06-08 12:53 PM
Hi, jonas
I've been working on the launchOperation function but it's giving me the bad parameter error all day. This is how my signature looks like. [DllImport(''STDFUPRT.dll'', EntryPoint = ''STDFUPRT_LaunchOperation'', CharSet = CharSet.Auto)]public static extern UInt32 STDFUPRT_LaunchOperation(ref STDFUPRT.DFUThreadContext Context, ref UInt32 Operation);I am not sure if I should pass the pointer as we did before for Mapping.Another Question is for the Operation Code what number did you pass? I passed 3 as they did in the source code. Also do you know what the variable TarSel does? there is no reference whatsoever in the manual2012-06-11 12:26 AM
Your signature is okay - nothing wrong with that. How does your DFUThreadContext struct look like? I did receive the same badparameter-error like I wrote some post ago and therefore looked through the source code of STDFUPRT_LaunchOperation(). There is only one way to get that error: Context.Operation must be anything else than 0 - 4. I used to set Operation to 3 (erase). If you set bDontSendFFTransfersForUpgrade to false the error doesn't show up (but I get an access violation). So I assume the size of the Operation-value must be 4 and not 2 like UM384 tells us.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.