2012-04-12 1:26 AM
To integrate firmware update functionality into a custom c♯ application I start to use ST Dfuse dll from c♯. I managed to enumerate and identify the device (UM0392 - 3.1 and 3.2) but now get stucked while trying to erase the device. Out of the manual:
DWORD OperationCode; PDWORD pNbAlternates; PMAPPING pMapping; PHANDLE pHandle; // Programming the operation contex lstrcpy(Context.szDevLink, DFUName); Context.DfuGUID=GUID_DFU; Context.AppGUID=GUID_APP; Context.Operation=OPERATION_ERASE; Context.bDontSendFFTransfersForUpgrade= TRUE; STDFUPRT_CreateMappingFromDevice((LPSTR)(LPCSTR)DFUName,&pMapping, &NbAlternates); STDFUFILES_CreateImageFromMapping(pHandle, pMapping); STDFUFILES_FilterImageForOperation(hImage, m_pMapping+TargetSel, OPERATION_ERASE, FALSE); Context.hImage=hImage; if( STDFUPRT_LaunchOperation(&Context, &OperationCode) != STDFUPRT_NOERROR) { Printf(�Erase error�); } The call of STDFUPRT_LaunchOperation() does always return a STDFUPRT_BADPARAMETER error. Is there a way to get some more information about this error? Which parameter is bad? The first parameter in LaunchOperation() is a pointer to the struct DFUThreadContext. I rebuilt this struct in c♯ using the information given in UM0384.pdf chapter 4.3.4. My UM0384 is revision 1 - June 2007 - wonder if that user manual is still up-to-date?!? I did not find UM0384 on the webpage (my copy is out of the package UM0412.zip). Does anyone have a newer one? Thanks in advance for any help #st-dfu #st-dfuse #dfuse2012-08-29 6:51 AM
Hi Arthur,
Please try the following implementation: private Mapping[] getDeviceMemoryMapping() { int stRetVal; /*ST's error code*/ int numberOfAlternates; /*The number of memory units that are exposed for DFU operations*/ bool sectorsInitialized; /*Monitor the sector initialization process*/ byte[] devLinkArray; /*Holds the device path*/ IntPtr pMapping, currentMapping, pDevLink; /*Various pointers*/ GCHandle byteArrayHandle; /*Prevent GC from moving the byte array while passing its address*/ DFU_Mapping dfuMapping; /*ST's mapping structure*/ Mapping[] mapping; /*return value*/ mapping = null; stRetVal = 0; numberOfAlternates = 0; sectorsInitialized = true; pMapping = IntPtr.Zero; pDevLink = IntPtr.Zero; dfuMapping = new DFU_Mapping(); devLinkArray = new byte[Utilities.BUFFER_SIZE]; /*Prevents GC from moving devLinkArray while it's address is passed to ST's unfriendly function*/ byteArrayHandle = GCHandle.Alloc(devLinkArray, GCHandleType.Pinned); try { pDevLink = Marshal.UnsafeAddrOfPinnedArrayElement(devLinkArray, 0); Marshal.Copy(new ASCIIEncoding().GetBytes(usbDevice.Path), 0, pDevLink, usbDevice.Path.Length); stRetVal = DFU_Wrapper.STDFUPRT_CreateMappingFromDevice(ref devLinkArray[0], out pMapping, ref numberOfAlternates); if (stRetVal == (int)DFU_FilesReturnCodeType.NoError && numberOfAlternates > 0) { currentMapping = pMapping; mapping = new Mapping[numberOfAlternates]; for (int i = 0; ((i < numberOfAlternates) && sectorsInitialized); i++, currentMapping = Utilities.IncrementIntPtr(currentMapping, Marshal.SizeOf(typeof(DFU_Mapping)))) { dfuMapping = (DFU_Mapping)Marshal.PtrToStructure(currentMapping, typeof(DFU_Mapping)); mapping[i] = new Mapping(dfuMapping); mapping[i].PMapping = currentMapping; sectorsInitialized = mapping[i].InitializeSectors(); } } else/*ST error or illegal state*/ { if (stRetVal != (int)DFU_FilesReturnCodeType.NoError) onDeviceError(usbDevice.Identifier, ErrorType.DFU_CouldReadMemoryMapping, new object[] { stRetVal }); else onDeviceError(usbDevice.Identifier, ErrorType.DFU_CouldReadMemoryMapping, new object[] { ''Memory units for DFU usage were not found'' }); } } catch (Exception e) { mapping = null; onDeviceError(usbDevice.Identifier, ErrorType.DFU_CouldReadMemoryMapping, new object[] { e.Message }); } finally { byteArrayHandle.Free(); } return mapping; }Hope this helps,Assaf2012-08-29 7:02 AM
2013-01-18 7:36 AM
Hi,
I'm also trying to write some C# code to do the ST DFU erase and download. What you've got here looks very useful ,and I'll have a dig thru it on Monday, but I wondered if any of the posters had a complete working .net app they they could post somewhere (eg. Code Project), I'm sure it would be very useful to other people too. Cheers, MarkWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.