2019-03-05 1:20 AM
Hi
For some time I have been using the ST-Link programmer from a NUCLEO-L452RE board for programming a custom STM32 board (external MCU). It has been working very well.
Recently, I have acquired a NUCLEO-L452RE-P, which has a bit different ST-Link programmer. For instance, it uses a micro USB connector as opposed to a mini connector. Also, it has an extra jumper. But aside from that, they look pretty much the same.
The thing is, I cannot get the NUCLEO-L452RE-P programmer to work on the same custom STM32 board. I have connected it the same way as I do for the NUCLEO-L452RE using the same SWD cable. Both ST-Link programmers have the same (latest) firmware V2J33M25.
I use Atollic TrueSTUDIO which reports the following error:
Error in initializing ST-Link device.
Reason: (4) No device found on target.
Can anyone explain why they are not compatible?
Thanks
/ abaldur
Solved! Go to Solution.
2019-03-07 1:57 AM
Thx, will try that. However, I don't have that connected on the NUCLEO-XXXXRX variant where it works?
/ abaldur
2019-03-07 2:17 AM
The issue is the same.
I have now mounted a 100 ohm resistor on R23 and soldered a wire from CN3.Pin1 (VDD_TARGET) to 3V3_ST_LINK.
/ abaldur
2019-03-07 5:47 AM
Well, sorry, I don't know now... I have an ST-LINK cut from an MB1319B on my bench. It is working, I'm currently connected to a STM32F7.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.