2019-03-05 1:20 AM
Hi
For some time I have been using the ST-Link programmer from a NUCLEO-L452RE board for programming a custom STM32 board (external MCU). It has been working very well.
Recently, I have acquired a NUCLEO-L452RE-P, which has a bit different ST-Link programmer. For instance, it uses a micro USB connector as opposed to a mini connector. Also, it has an extra jumper. But aside from that, they look pretty much the same.
The thing is, I cannot get the NUCLEO-L452RE-P programmer to work on the same custom STM32 board. I have connected it the same way as I do for the NUCLEO-L452RE using the same SWD cable. Both ST-Link programmers have the same (latest) firmware V2J33M25.
I use Atollic TrueSTUDIO which reports the following error:
Error in initializing ST-Link device.
Reason: (4) No device found on target.
Can anyone explain why they are not compatible?
Thanks
/ abaldur
Solved! Go to Solution.
2019-03-07 5:47 AM
Well, sorry, I don't know now... I have an ST-LINK cut from an MB1319B on my bench. It is working, I'm currently connected to a STM32F7.
2019-03-05 1:26 AM
I see CN2 jumpered on both boards. To program an external device, you need to remove them. Pehaps you did that, but you did not mention, so just in case.
2019-03-05 1:35 AM
The new part number and the different appearance suggests the manual was updated as well. Did you check ?
I wouldn't bet on it, though ...
2019-03-05 1:38 AM
Hi Uwe. Thx for the quick reply. The CN2 jumpers have been removed. On both ST-Link programmers, I have removed ALL jumpers. Only the SWD connector and the UART connector is used. That is CN3 (SWD) and CN4 (UART) on NUCLEO-L452RE-P and CN4 (SWD) and CN3 (UART) for NUCLEO-L452RE.
2019-03-05 1:52 AM
Hi AvaTar. I have looked in the user manuals for both boards (UM1724 and UM2206). I have not been able to find anything that could explain it.
2019-03-05 2:31 AM
I have neither of your L452 Nucleos - already too much of those boards, and too little time.
Have you reviewed the schematic (of the new board), especially the SWD connection, and cross-checked the board/PCB with the schematics ?
ST's documentation department seems to have a little backlog recently.
2019-03-06 8:08 AM
2019-03-07 1:10 AM
Hi @Mike_ST
The ST-Link is separated from the target board.
I have connected my external MCU to the following pins on the SWD connector (CN3):
The rest is left unconnected, and the target MCU is powered separately from a 5V USB supply.
I have tried populating the R23 resistor (which was mounted from factory on the NUCLEO-XXXXRX variant). The result is the same:
Error in initializing ST-Link device.
Reason: (4) No device found on target.
/ abaldur
2019-03-07 1:14 AM
..
2019-03-07 1:14 AM
You absolutely need to connect pin 1 on CN3 connector. If I'm correct, it is an input that sense the target MCU voltage 1.8 or 3.3V. So please connect to 3.3V
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.