2023-06-24 1:05 PM - edited 2023-06-24 1:06 PM
I have this board (revision C-04) with ST-LINK removed (PCB cut off), so the power 3V3 is supplied from CN7. It works fine, but the red power led (LD3) also works. LD3 is, I think, connected to the 5V net, and 5V to 3V3 regulator should not be working but then why the LD3 is shining red?
Solved! Go to Solution.
2023-06-24 10:54 PM
> 5V to 3V3 regulator should not be working
Many LDOs have built in reverse diode from output to input.
JW
2023-06-24 10:54 PM
> 5V to 3V3 regulator should not be working
Many LDOs have built in reverse diode from output to input.
JW
2023-06-26 8:19 AM
I checked the datasheet, but I didn't see something like that. It makes sense, thanks.
2023-06-27 6:58 PM
In this case, the SB2 should be removed to avoid any damage for LDO.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.