STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Powering NUCLEO-H743ZI2 with User USB?

I'm currently working on a project involving a NUCLEO-H743ZI2 board.I want to know if it's possible to power the board with User USB instead of ST-Link USB.Or if it's possible to transfer data using ST-Link USB and use User USB for debugging.Thank yo...

JJ.5 by Associate III
  • 8199 Views
  • 15 replies
  • 0 kudos

i couldnt figure out how to post to ideas but i would love if st would make a version of the st link v3-mods that didnt have to usb connector on it and break out the usb input for programming

as with the stlink mods your limited to a 5v out at 200ma and if the usb was broke out i could use a usb c connector on a pcb and have alot more voltage options

What is the T_SW_DIR pin on STLINK-V3?

I can't find any information about what the T_SW_DIR pin is on the STLINK-V3 products. I am planning to use a STLINK-V3MODS programmer in a project, but I can't find any other information about this pin, other than it is an output. Does anyone know w...

sean123 by Associate
  • 2570 Views
  • 3 replies
  • 0 kudos

I am now using 1.8V for VDD and 3.3V for VDDA. There is no USB. So I am fine having this power regime. The question I now have is on the programming aspects of the MCU (STM32G4A1KEU6). I have (we use) an STLINK programmer:STLINK-V3MINIE. All these time I

I am now using 1.8V for VDD and 3.3V for VDDA. There is no USB. So I am fine having this power regime. The question I now have is on the programming aspects of the MCU (STM32G4A1KEU6). I have (we use) an STLINK programmer:STLINK-V3MINIE. All these ti...

DOwus.1 by Associate II
  • 2621 Views
  • 2 replies
  • 0 kudos

Resolved! How to control STLink from cli, or python?

Hi, I need to control Stlink form python code.1) On some PC I am not able to connect with STLink to my MCU - I tried STM32CubeProg and ST-Link utility. The Error is  UR connection mode is defined with the HWrst reset mode.But why on the same PC the S...

JR2963 by Senior II
  • 11757 Views
  • 9 replies
  • 1 kudos

Designing with STM32L496

Hello Team,We are planning to use the MCU STM32L496QGI6 for one of our new projects.The MCU will be powered from a 1.8V source (since all external peripherals are working in 1.8V only).One of the SPI slaves is working in 3.3V, so we are planning to u...

shibin by Associate II
  • 907 Views
  • 1 replies
  • 0 kudos

St-Link error (DEV_USB_COMM__ERR)

Hello We brought new St-Link/V2, Now I tested with STM32CubeProgrammer , In this we unable to read serial number of this St Link (some time it shows '@' symbol) . please check the attached the .png file Same issue we found in working ST-Link pre...

_legacyfs_online_stmicro_images_0693W00000dDHFAQA4.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.