2020-01-29 4:37 AM
The other i have lights up and connects nice to PC.
Is there a schematic for finding the fault, or some way to re-load the firmware?
2020-01-29 1:53 PM
Another ST-LINK/V3, or something else?
Try a different cable, not a charging cable.
Try a different port, avoiding hubs or docking stations.
Try a different PC
No schematic, but might look at NUCLEO-H743ZI2 or H747I-DISCO using an ST-LINK/V3
2020-01-29 2:21 PM
I have 2 ST-Link - in total same setup, same cable etc. 1 is working and enumerates the disk drive and lights led LED - The other is dead.
Both was complete news from the box. the only difference is the first broken was connectes to the target, this eval board, with a 20pin ribbon cable from an old ULINK2... i suppose that would fit... Yet i havent tried number 2 STlink on the eval board...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.