cancel
Showing results for 
Search instead for 
Did you mean: 

My STLINK V2 debugger is giving "error: Target not connected" while flashing in STM32F401VBT6 controller? Please tell me the default connections of STM32F401VBT6 while flashing and debugging?

ASawa
Associate II

I have given 3.3V to all VDD,VDDA,VBAT,VREF+ with capacitive filtering (100 nf & 1uf) as per datasheet. BOOT0 pin is connected to GND. SWDIO and SWCLK connected to debugger pins. Still it is giving same error.

when BOOT0=1, flashing is done but it gives debugging problem.In debugging mode, debugger does not display data of registers.

Please give me the solution for this error.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Make sure the ST-LINK/V2 Pin 1 or 2 are connected to VDD

Check signal level on NRST

Check voltages on VCAP pins

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ASawa
Associate II

recommend voltages on vcap1 and vcap2 for stm32f401vbt6

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.