2020-03-23 6:25 PM
2020-03-23 11:32 PM
Has this CPU/Board ever worked or connected properly?
Is the NRST pin connected on the debug interface?
Try connecting when BOOT(0) pin is HIGH
2020-03-24 1:06 AM
Yes, the signal is connected properly. Connect the 20pin cable to ST_LINK. It can be debugged with ST_link. But can't debug with J link
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.