2025-07-09 4:14 AM - last edited on 2025-07-09 4:18 AM by Andrew Neil
we need to connect a camera to the STM32H745-Disco board. Our ultimate goal is to develop an application similar to the image_classification example from the STM32AI Model Zoo. Since we are unable to purchase another board, we would like to ask if it is possible to connect a camera module to the STM32H745-Disco for this purpose. Any guidance or suggestions would be greatly appreciated.
2025-07-10 12:41 AM
As no camera connector available on STM32H745-Disco board, even DCMI interface is supported by STM32H745XI on this board, I think it may not possible to connect it to a camera module or very complex to do it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.