2024-01-04 11:08 AM
Hello,
I have programmed a Nucleo-L476RG with the Blinking LED example. Until there is all fine.
Now, I want to load a new program on the board. Windows Explorer and ST-Link do not detect the board and cannot load a new program on the board.
I bought the same board again. It is detected immediately by Windows Explorer and the ST-Link.
I see one visual difference between the two boards: The LD1 in the "non-detected" board is permanently green while the LD1 in the detected board is permanently red.
Could you give me advise have to bring the board to a state where I could load a new program again?
Thank in advance.
2024-01-05 6:31 AM
Hello,
Try to connect (under reset) to the board with the STM32CubeProgrammer, and to erase the MCU to check if it is the Blinking LED example that makes troubles.
2024-01-11 11:11 PM
STM32CubeProgramer do not detect the board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.