2025-05-28 11:56 AM
Hello ,
Does anyone use STM32F429i eval board ?
The user manual (shown as the screenshot below) for my F429 eval board says it has 4 USART ,4 UART. But I can only find 1 DB9 male port marked as USART1.
Also, when I use CubeIDE to configure USART1, it automatically enabled PB6 and PB7 for TX and RX. But on the user manual , the schematic clearly says RS232_TX for USART1 is PA9, RS232_RX is PA10.
That's really confusing...
I am not able to find 4 USART connections, nor can I configure the right PIN numbers for USART1.
I tried to verify the Pin numbers from the github example folder, it seems they don't have the PIN number either.
Solved! Go to Solution.
2025-05-28 1:06 PM
A USB to UART adapter has been used by many, rather than using RS232, e.g.
https://ftdichip.com/products/ttl-232rg-vip-we/
Most Nucleo boards connect one of the micro's USARTs to the on-board ST-LINK debugger, which provides a Virtual Com Port ("VCP").
2025-05-28 1:14 PM
It is a good option too.
Thank you!
2025-05-28 4:01 PM
Thank you for pointing out the table!
I am using the same PDF file.
The table does show 4 U(S)ART PINs. But those PINs might be referring to the STM32F4 chip like @Pavel A. mentioned. Right now I think only USART1 is available for communication between the board and PC.
2025-05-28 5:33 PM
Yes, the STM32429I-EVAL board provides only USART1 via the RS232 or IRDA connection.
Other might be possible via the pin headers, but most everything looks to be committed to screens, external memory,etc.
I think this uses the ST-LINK/V2 and predates the V2-1 model with the VCP support. It's a rather old board design, originally from 2013
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.