2024-03-02 1:33 AM
Hello Guys,
I am using waveshare 4.3 inch e paper UART display module. I looked to manual thousand time and I found a library called epd. this library was written in cpp and I rewrote for my stm32f411RE nucleo board in c and HAL Library. Buffer working good and I am transmitting hex codes to my computer. But the screen doesn't respond to these commands. I need for your help. My files and displays wiki are attached.
Thank you!!
https://www.waveshare.com/wiki/4.3inch_e-Paper_UART_Module
2024-03-02 7:29 AM
Not sure there are a lot with the hardware to do the debug for you.
The IsSend will need to be volatile if changed in interrupt/callback.
Perhaps add diagnostic / telemetry output via serial so you can observe the interactions between the STM32 and display. Use a scope or logic analyzer to check the hardware level interactions.
2024-03-02 12:12 PM
Here you can get help with this.
2024-03-03 3:49 AM
Thank you for your answer!!
I am sending data to display via USART2 which connected both pc and display and I observed the data that board send to display. At the pc side everything fine but display doesn't respond.
wiki says there is a parity bit but it is in the library. should I set a parity bit by cube mx? but I don't know how to set that because wiki doesn't say what parity is that (odd or even).
2024-03-03 3:56 AM
You can try it - just set (in cubemx) in usart2 parity , then try.
If still no response, change odd/even and try again.
2024-03-03 11:47 AM
Current set to no-parity, ie 8N1
/**
* @brief USART2 Initialization Function
* @PAram None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
2024-03-04 4:58 AM
it didnt work bro
2024-03-04 4:58 AM
ı try both of them it didnt work
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.