2024-05-24 6:08 AM - last edited on 2024-05-24 10:47 AM by Tesla DeLorean
Hey everyone,
I want an UART communication between my PC and my STM32H745 Disco board.
By default the UART 3 (connected to STLINK connector) is one core M4.
My baud rate is 115200. My pins are initialized by default.
My main is this :
and the hal_uart_transmit function returns HAL_OK.
On my computer, with Putty, i can't see the data sent.
Can you help me with this ? :)
Solved! Go to Solution.
2024-05-24 6:50 AM
2024-05-24 6:49 AM - edited 2024-05-24 6:53 AM
Hello @fru999 ,
Please make sure that the UART configuration in your code matches the settings in Putty: baud rate, word length, parity.
Could you please take a look at this wiki: Step3 Introduction to the UART may help.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-24 6:50 AM
Pin pour UART 3 sur STM32H745 DISCO sont :
TX : PB10
RX : PC11
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.