2023-10-23 3:40 AM
Hi.
After firmware upgrade for st-link v2, windows computer recognized the st-link as universal serial bus instead of virtual com port. whenever i try to program to MCU, there is error like a "No target device found".
How can I solve it?
Below image is the device manager to be recognized as Universal serial bus. there is no PORT.
Thank advance.
BR
2023-10-23 4:52 PM
Ok, but the diode suggests that you expect the ST-LINK to power the 3.3V whereas the expectations for the buffers is that your target powers them. Check the voltage you see on pin 1/2 of the 20-pin header
2023-10-23 4:58 PM
Hi Tesla,
You mean that the target board should provide the power 3.3V to the st-link VDD pin 1/2 of the 20-pin header.
or,Is 3.07V little bit low voltage for flashing?
Thanks
Regards,
2023-10-23 6:55 PM
Hi
After measuring the voltage of 1/2 of 20-pin header with tester, the value of voltage is 3.13V.
Thank you.
Regards,
2023-10-25 4:57 PM
Hi,
MCU is STM32L072CZ.
Boot0 is to wired with GND. Now Voltage is 3.25V for VDD : 3.25V, SWDIO, SWCLK, nRST, RST.
Even if I tried to connect with My MCU Board which housed STM32L072CZ, it didn't connect with them.
Please help me.
thank you in advance.
Kevin
2023-10-25 5:12 PM
Hi
Error message is as below if i used the stm32cubeprogrammer.
09:10:59 : UR connection mode is defined with the HWrst reset mode
09:10:59 : ST-LINK SN : 51FF6D066684504828451087
09:10:59 : ST-LINK FW : V2J42S7
09:10:59 : Board : --
09:10:59 : Voltage : 3.25V
09:10:59 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
Thank you in advance
Kevin
2023-10-25 6:15 PM
Hi
Below is image for ST-Link for nRST and SWCLK when i tried to connect with MCU using STM32Cubeprogrammer.
2 blue channel is nRST, 1 yello channel is SWCLK.
Thank you.
Best Regards,
2023-10-25 6:39 PM
Hi
Below is SWDIO, SWCLK waveform when I tried to connect with MCU using STM32CubeProgrammer.
Thank you.
BR
2023-10-25 6:43 PM
Blue 2 channel and yellow 1 channel are little bit malfunction to measure the voltage.
Thank you.
BR
2023-10-25 9:40 PM - edited 2023-10-25 9:42 PM
Is there some issue with the grounding here?
Your diagram here has GND and SWDIO switched. Is the wiring harness correct?
2023-10-25 10:44 PM
Hi Tesla,
In first picture, The oscillator is liitle bit malfunction to measure the voltage as you indicated.
However, second picture is good to measure swdio, and swclk waveform.
Thank you.
BR
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.